NSK show us life under the hygiene regime
Hygiene is the key ingredient in food and beverage manufacturing. Complying with stringent hygiene s...
Corrosion, erosion, cavitation and mechanical damage all cause wear to pump castings, impellers and volutes. But they can all be effectively and economically repaired with ERIKS know-how and Henkel’s Loctite® surface engineering products.
ERIKS and Henkel have worked together over many years to repair, improve and upgrade customers’ pumps, and achieve significant savings.
For example, ERIKS evaluated a major UK automotive manufacturer’s 22kW ELPO process water pump as under-performing by at least 30% against the original specification. Dismantling the unit revealed heavy corrosion, a worn, burred and imbalanced pump impeller, seized mechanical seal, and pump/motor misalignment. The volute was cut-water worn, the bearings showed evidence of fretting and corrosion, and the motor was not inverter rated.
Engineers at ERIKS’ Southampton EMS workshop repaired and restored the pump to efficiency in just 7 simple steps:
ERIKS’ remedial work restored the pump to its original specification, increasing its efficiency by 30%. The repair cost was £5,542, but this was largely offset by a reduction in energy costs of £3,936 in the first year alone.
Under the Government’s Enhanced Capital Allowance scheme for investment in energy-saving equipment, the customer also reclaimed £585.90. So the real cost of the repair was just £685. Long-term savings of carbon emissions (28 tonnes over 5 years) and energy 51.90MWh) will total £19,680 – on one pump alone.
Loctite® polymer composites, coatings and compounds protect parts against attack. Formulated with ceramic fillers for excellent wear resistance and superior adhesion, they can create a sacrificial and renewable working surface, protecting the structural integrity of the original substrate.
Suitable for all surface sizes, and with none of the heat stress associated with traditional methods, they are able to:
The Loctite® range provides a choice of grades – for fine particles through to coarse – in brushable, sprayable and trowelable formulations, with typical temperature resistance from -30◦C to +120◦C across the range. (Special grades can be used up to 230◦C.)
Loctite® PC 7118 ceramic wearing compound, for example, conforms to KTW guidelines and for direct contact with cold, potable water. It can be used to protect against wear and corrosion for any industrial device carrying potable water. At the same time, it provides high vertical sag resistance and very high abrasion resistance.
Or for use on lining tanks and chutes, heat exchangers, condensers, cooling pump impellers, rudders and pintle housings, there’s Loctite® 7255 energy-efficient coating. With WRAS UK approval, this ultra-smooth, ceramic reinforced epoxy provides a high gloss, low friction coating to seal and protect.
But don’t just take Henkel’s word for it. A Humber refinery reported an 8% energy saving resulting from application of this coating.
For more information on Flow Control solutions and to get in touch with one of our ERIKS Pumps Specialists or Valve/Flow Control Engineers, please contact your local ERIKS Service Centre, who will be happy to discuss your options.
#Loctite #Henkel #Solutions #Pumps #Coatings #Engineering #Adhesives
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
Hygiene is the key ingredient in food and beverage manufacturing. Complying with stringent hygiene s...
For all general enquiries use the Enquire Online form - we'll connect you with the best member of our team for your query. Alternatively, look up your local service centre...
We are proud to boast a strong team of technical specialists in each of our product and service areas. If you have a technical question a member of our team would be happy to help.
At ERIKS we strive to deliver the best quality service and products. As part of this goal we encourage customers to submit feedback on their experiences so we can resolve any issues and concerns.