Precise and Rapid Positioning with the EPCC Electric Cylinder from Festo
- Mark StoneFor simple, affordable and accurate positioning, the EPCC electric cylinder from Festo is hard to be...
Traditionally, the cure for an inefficient belt drive has been to simply replace the worn one with a new one. However, Gordon Smith, ERIKS Product Manager for Open Drives, argues that the replacement of a pulley is a far more effective way to resolve your problems.
Remarkably, as many as 50% of new belts are actually fitted to worn pulleys. Pulleys are just as susceptible to wear and tear as they go through the rigours of everyday life, yet in so many cases, their condition is overlooked and passes right under the nose of the manager.
With that in mind, it must be stressed that determining a pulley’s condition is not a difficult task, nor does it require any expensive tools or machinery. A simple tool in the form of the Fenner Pulley Groove Gauge – which can fit onto any keyring – is enough to determine whether a pulley actually needs to be replaced.
Simply clean off a section of the pulley and insert the appropriate width gauge profile into the groove, and if there’s more than 5% wear on the pulley’s pitch-line, then it needs to be replaced. Another good rule of thumb is that when the gauge is inserted, there should be no visible gaps at the sides.
You should also bear in mind, if there are any gaps or movement, this indicates that the belt isn’t sitting flush with the pulley and therefore it’s unable to produce the optimum amount of friction to operate the drive as efficiently as possible.
In reality, replacing a worn belt but ignoring pulley condition will do little to improve the efficiency of a drive, but it will reduce the life of the new belt. And, from a financial stand-point, poor drive efficiency will have a significant impact on both overall plant production and energy bills.
Although it’s inevitable that pulley damage will occur, correct installation remains key. Research has suggested that 70% of belt friction drives are actually incorrectly installed – which is quite an astounding figure.
Firstly, the maintenance manager must ensure that the most appropriate drive has been chosen. This will ensure the use of fewer belts and will reduce loading on machine bearings, increasing the systems lifespan and reducing potential downtime.
Once the correct drive has been selected, it must be installed effectively. Alignment is key and there are various ways to test this – From holding a taught piece of string across the pulley faces in different positions, to the most effective way, the Fenner laser alignment gauge.
By making use of the correct available tools, the drive is far more likely to deliver its maximum rated power, at its premium efficiency.
In addition to correctly choosing and installing the most appropriate drive for your application, it’s advised that you conduct regular health inspections. These are neither difficult nor time-consuming. If you are looking to conduct these audits independently, I would recommend storing a full belt efficiency kit on site, such as the one from Fenner, which includes a belt tension indicator, a drive alignment laser and a pulley groove gauge.
Given the frequency of belt drives in industrial applications, it’s vitally important that maintenance managers pay equal attention to the pulley and the belt, right through to installation and planned checks – only then will you truly reap the rewards of an optimised and highly efficient belt drive system.
For more information please call us on 0121 508 6000 or visit www.fptgroup.com
An essential item for your engineering toolbox, get yours today - no catch, we're just happy to help.
Get the latest updates from ERIKS including:
Choose any or all of these via the ERIKS Subscription Centre!
Our Know+How brings together the best of the latest Know+How Hub articles in one easy to digest magazine, covering the following topics:
That's why its the leading magazine for maintenance engineers from ERIKS.
Want Know+How Magazine delivered direct to your door? Visit the ERIKS Subscription Centre to opt-in!
Take a look at our latest updates...
For simple, affordable and accurate positioning, the EPCC electric cylinder from Festo is hard to be...
For all general enquiries use the Enquire Online form - we'll connect you with the best member of our team for your query. Alternatively, look up your local service centre...
We are proud to boast a strong team of technical specialists in each of our product and service areas. If you have a technical question a member of our team would be happy to help.
At ERIKS we strive to deliver the best quality service and products. As part of this goal we encourage customers to submit feedback on their experiences so we can resolve any issues and concerns.