Taking a step in the right direction with Schaeffler
We are all becoming more aware of the need to protect the world from catastrophic climate change. Th...
Although most conveyor chains these days are wedge riveted as standard, the option to specify spin riveting is an important one and should be considered for critical applications both by designers of original equipment and maintenance engineers alike.
It’s an important consideration and an effective solution on applications where attachments have been fitted to the side plates of conveyor chain that could be carrying heavy loads. In fact, Alec Annand, the manager of Renold Chain’s Customer Service Centre, recommends that all engineers specifying custom designed conveyor chain, with attachments, should consider the benefits of spin riveting as an option, due to the extra side plate security it provides.
The recommendation comes after one manufacturer using a large amount of conveyor chain, at one of its plants, sent an inspection team to Renold Chain’s Bredbury Service Centre, which also produces both transmission and conveyor chain to exact specifications to a wide range of industries including OEMs, theme parks, packaging, printing and food, to check on the quality of its spin riveting process.
Conveyor chain operated by the manufacturer was fitted with attachments that had to carry very heavy loads through underground chambers that were inherently dirty and foul smelling.
The load on the chain side plates was causing them to work loose over time and eventually they would come off. An engineer would then have to descend into these dark, unpleasant chambers to carry out repairs.
The maintenance team at the manufacturer took the decision to specify replacement conveyor chain with spin riveted side plates as a solution. Not only would this virtually eliminate the need for engineers to enter the unpleasant environment to carry out repairs, but the spin riveted chain would also cut maintenance and increase productivity.
Wedge riveting is cheaper and quicker than spin riveting, which is why most conveyor chain manufacturers have adopted this process as standard. It’s fine on most applications, especially where the side plates are not fitted with load carrying attachments, but spin riveted conveyor chain provides enhanced side plate security, and as Annand recommends, it should be considered for all critical applications.
During the spin riveting process, at Renold’s customer Service Centre, the pins are end softened to prevent cracking during riveting, and to provide easier onsite installation, riveting and dismantling for customers. The spin rivet itself has a mushroom-like head and provides much greater surface area contact with the side plate. It is this feature that provides the required enhanced security of the chain’s side plates.
For more information on Power Transmission solutions and to get in touch with one of our ERIKS Chain Specialists or Power Transmission Engineers, please contact your local ERIKS Service Centre, who will be happy to discuss your options.
#SpinRiveting #Printing #Packaging #Food #Conveyor #Chain #Plates #Engineering #ERIKS #LetsMakeIndustryWorkBetter
Rising demand for energy in industry is leading to a parallel rise in CO2 and CO2 equivalent emmission. Governments worldwide are seeking ways to reduce these emissions.
Since electric motors consume 46% of electricity generated worldwide, governments are introducing legislation to make electric motors more energy-efficient, which will reduce their energy consumption and in turn their CO2 and other emissions.
Following the introduction of a voluntary scheme in 1999, the EU agreed a Directive defining a timeline for the introduction of Minimum Energy Performance standards for induction motors. This regulation will be repealed from July 2012 and replaced over the period to July 2023 with new energy-efficiency requirements for a wider range of motors.
Download a copy of our latest whitepaper that explains what this will mean to you and your plant.
Get the latest updates from ERIKS including:
Choose any or all of these via the ERIKS Subscription Centre!
Our Know+How brings together the best of the latest Know+How Hub articles in one easy to digest magazine, covering the following topics:
That's why its the leading magazine for maintenance engineers from ERIKS.
Want Know+How Magazine delivered direct to your door? Visit the ERIKS Subscription Centre to opt-in!
Take a look at our latest updates...
We are all becoming more aware of the need to protect the world from catastrophic climate change. Th...
For all general enquiries use the Enquire Online form - we'll connect you with the best member of our team for your query. Alternatively, look up your local service centre...
We are proud to boast a strong team of technical specialists in each of our product and service areas. If you have a technical question a member of our team would be happy to help.
At ERIKS we strive to deliver the best quality service and products. As part of this goal we encourage customers to submit feedback on their experiences so we can resolve any issues and concerns.