Earplugs to shout about with 3M
Have you heard? There’s a revolutionary new earplug available. According to Bryan Myers – 3M’s Busin...
Whatever recipe you are blending, mixing or formulating - food, beverage or pharmaceutical - there's one ingredient that can put the whole process at risk. A human. So introducing an automated in-line or batch blending system to the mix will increase efficiency, productivity and repeatability of your process. And if it's an ERIKS system, it can do even more.
Humans are fallible, inaccurate and slow. In production processes which demand repeatability, accuracy and speed, that makes them a liability.
The solution is an automated batch or in-line blending or mixing system, for fast, accurate dosing, time after time. All at a speed that significantly accelerates productivity.
From a single production line upwards, ERIKS Flow Control can design, install and maintain a cost-effective system for your application. And because ERIKS is a major purchaser of high-quality brand-name system components, it will be built-to-order, but at a close to off-the-shelf price.
Moving from a batch production process to an in-line system delivers a wide range of benefits. That's because manually-operated batch blending and mixing systems have an inherent set of problems.
ERIKS is currently undertaking design and installation of a new in-line system for a manufacturer of flavoured and infused oils. A number of issues with their current batch system should be resolved as a result.
The customer produces small runs of speciality oils, currently hand-blended to the required ratios and specifications, in 1000kg batches stored in intermediate bulk containers (IBCs). Product demand is high, and there is a large number of flavour variants, so the customer processes approximately 2,500 IBCs annaually - each one taking around an hour to blend.
Once an IBC has been blended, it has to be moved manually from the bulk oils dispatch point to the filler point on the production line. This involves manual handling on a trolley, over a distance of around 150m.
Moving IBCs is a tipping and manual handling safety risk, and in the confined space around the production line poses the additional risk of machinery damage. The operation also takes the depalletiser operator away from his machine for at least 10 minutes at every IBC change. Since one of the lines involved can process a full IBC every 90 minutes, this is a significant amount of the operator's time which could be better used.
One final inefficiency is the 12 litres of oil lost from production at every oil change.
As part of the Project Definition presented to the customer, ERIKS itemised the main benefits the in-line system would achieve, together with the associated cost savings.
It doesn't matter how unusual or complex your mixing or blending requirement is, ERIKS can make it more efficient, accurate and cost-effective.
The specialist knowledge to design and build an effective in-line or batch system is only the start. To ensure reliability, the system will be engineered with quality components from well-known manufacturers. These include Xylem for pumps and Prominent for dosing systems, WEG for electric motors, Econ for valves and proportional valves, and Fenner for control systems.
And ERIKS' comprehensive Flow Control systems know-how, together with expertise in pumps, valves, flow meters, mixing vessels and weighing and dosing equipment, means you can source a complete system from one supplier. A supplier who also has the buying power to keep component costs down.
This all-in-one offering extends to the system itself: fully assembled and mounted on a compact stainless steel framework skid - together with the control panel, pipework, wiring, and inlet and outlet pipework connections - ready for delivery and "plug and play" installation.
ERIKS Flow Control engineers can also return regularly to check the system is operating within your required parameters, and to recalibrate, service and maintain as necessary.
In fact, with whole-life support from ERIKS' dedicated Flow Control Technology Centre, the service and maintenance can be just as fast, effective, repeatable and reliable as your blending and mixing itself.
The complete range of flow control solutions available at ERIKS Flow Technology Centre comprises:
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
Have you heard? There’s a revolutionary new earplug available. According to Bryan Myers – 3M’s Busin...
For all general enquiries use the Enquire Online form - we'll connect you with the best member of our team for your query. Alternatively, look up your local service centre...
We are proud to boast a strong team of technical specialists in each of our product and service areas. If you have a technical question a member of our team would be happy to help.
At ERIKS we strive to deliver the best quality service and products. As part of this goal we encourage customers to submit feedback on their experiences so we can resolve any issues and concerns.