In this article
Plug, Play, Perform: A Smarter Way to Upgrade Clarifier Drives
In wastewater treatment, some of the most critical processes depend on systems that move at an almost glacial pace. Clarifier tanks, for example, rely on ultra-slow, continuous rotation – often just one revolution every 90 minutes – to keep flow steady while heavier solids settle out. When that motion stops, the whole process is at risk.
For one northern wastewater company, ageing clarifier drive systems were becoming a growing concern. Many had been in service for more than 30 years, built up from multiple components bolted together over time. What once worked reliably was now a patchwork of motors, torque limiters, belts, chains and multi-stage gearboxes – each one another potential failure point.
Too many parts, too much risk
The problems were familiar. Water ingress caused bearing failures. Belts and chains stretched or snapped. Couplings drifted out of alignment. Gearboxes ran inefficiently, generating heat and wear. Every failure meant downtime, reactive maintenance and disruption to a process that cannot simply be paused.
Worse still, there was little standardisation across the site. Each clarifier had its own bespoke arrangement, with unique mountings and components.
Spare parts couldn’t be shared, fault-finding took longer than it should, and maintenance teams were constantly firefighting rather than planning ahead.
The utility needed a better answer – one that reduced complexity, improved reliability and could be rolled out consistently across multiple tanks and sites.
Simplifying the drivetrain
Working closely with the customer, ERIKS set out to rethink the clarifier drive from first principles. The result was a fully integrated planetary gearmotor system designed specifically for slow-speed, high-torque applications.
Planetary gearboxes are compact by nature, spreading load across multiple contact points to reduce wear and improve efficiency. In this case, the gearbox and motor were directly coupled into a single unit, removing the need for belts, chains, torque limiters or secondary gear stages altogether.
Despite being compact – roughly the size of a kettle – the unit delivers the smooth, controlled torque needed to rotate large clarifier arms reliably, hour after hour.
Control, protection and flexibility built in
To add another layer of resilience, each gearmotor was paired with a Variable Speed Drive (VSD). This allows for controlled acceleration and deceleration, protecting the mechanical system from shock loads while providing torque limiting in the event of blockages or abnormal conditions.
The VSD also gives operators the flexibility to fine-tune rotation speed as process conditions change – a valuable advantage when dealing with variable flows and loads. It’s a small addition that delivers big gains in control, protection and future-proofing.
A scalable, ‘plug-and-play’ approach
One of the standout features of the solution is its scalability. ERIKS designed a universal mounting and adaptor plate that allows the same standardised drive system to be fitted across different clarifier designs and tank sizes.
For smaller tanks with lower torque requirements, fewer units can be used.
Larger tanks can be scaled up accordingly. The principle remains the same, wherever it’s installed.
This standardisation brings real operational benefits. Spare parts are simplified. Maintenance teams become familiar with one system instead of many. Response times improve, and inventory costs come down.
Minimal disruption, maximum confidence
Installation was designed to be as straightforward as the system itself. In most cases, the new drive can be installed within a day, either by ERIKS engineers or the customer’s own teams.
That means minimal downtime and no prolonged shutdowns.
For the wastewater treatment site in in the North of England the impact was immediate. Uptime improved, maintenance demands dropped, and the clarifier drives were transformed from a persistent risk into a dependable asset.
By replacing complexity with clarity, ERIKS delivered more than a component upgrade. The result is a scalable, off-the-shelf solution that improves reliability today, simplifies maintenance tomorrow, and gives water companies confidence that one of their most critical processes will keep turning – slowly, smoothly, and exactly as it should.
For more information on Water and Wastewater, or get in touch with your local ERIKS Service Centre who will be happy to discuss your options.
#ERIKSUKI #Wastewater #ClarifierDrives #RotatingEquipment #EngineeringSolutions
Beyond clarifier drives
See how ERIKS supports the water industry with engineered solutions and service.