In this article
More power to protect, in EV battery manufacturing
Forget the Electric versus Petrol debate. For workers in the electric vehicle battery manufacturing sector, the important issue is Electric versus People. Sector growth means more people are being employed in the manufacture of the EV’s lithium-ion battery. Which means more employees exposed to new risks and safety challenges, demanding new PPE solutions. Fortunately, the experience and the products are out there, just waiting to be plugged-in to your business.
Health and safety risks are inevitable in industry. As new industries, technologies and manufacturing techniques arise, so do brand-new risks. The manufacture of lithium-ion batteries for EVs creates a particularly challenging combination of an aggressive environment and a new set of risks.
Ansell have pioneered hand and body protection solutions for decades, so are naturally at the forefront in offering effective solutions to keep employees safe in this changing manufacturing landscape.
Step-by-step protection
The production of lithium-ion batteries can be broadly broken down into five steps:
- Electrode manufacturing
- Cell assembly
- Cell finishing
- Battery module assembly
- Packaging and transportation
At each stage, different hazards require different categories of protection. For example, there’s painful and potentially debilitating hand fatigue when handling materials and tools for placing cells. Or potentially fatal electric shock, when working with high-voltage components and wiring.
So at various stages of production, workers will require protection from abrasion, cuts and chemicals. ATEX, thermal and welding protection will also be needed at certain times. And protection can work both ways.
So during cell assembly, battery module assembly and cell finishing – conducted in cleanroom environments – employees need PPE to protect the product itself from contamination.
But even in this relatively new industry, some stages haven’t changed. Unloading and unpacking raw materials, and loading and transporting finished products, means – as always – risk of crush and pinch injuries and other material handling-related harms. These also need to be prepared for and protected against.
Protection at your fingertips
One type of protection won’t resolve all risks involved in lithium-ion battery production. Which is why Ansell produces a range of protective gloves and body protection equipment.
With Ansell’s expert guidance you can choose the right equipment for the particular challenges of every manufacturing stage, and give your employees the best possible protection at all times.
Chemical hand protection
Protect against exposure to chemicals during loading, mixing and coating, for example, with a selection of AlphaTec® gloves for use during electrode manufacturing and battery module assembly.
Cut protection
Cuts and lacerations are an issue when, for example, changing blades during electrode manufacturing. The HyFlex® 11-754/755/757 provides the hand protection needed, including for battery module assembly and battery packing and transportation.
Abrasion protection
Protection from abrasion is often necessary during battery module assembly, battery packing and transportation. The HyFlex® 11-561 provides up to 20% more abrasion resistance with improved FORTIX™ Technology.
Touchscreen / ESD protection
The HyFlex®11-819 ESD is EN 16350:2014 certified to protect products from electrostatic discharge – essential during battery module assembly. It is also touchscreen compatible.
Single-use protection
Various ‘one-off’ hazards arise during the manufacturing process, requiring a single-use disposable glove for quick and easy donning and disposal. Ansell offers a choice of TouchNTuff® gloves – for chemical splash protection or clean room environments, for example – and MICROFLEX® glove options, to meet all needs.
Electrical protection
Essential during electrode manufacturing, cell assembly and battery module assembly, effective electrical protection is offered by the ActivArmr® Rubber Insulated Gloves portfolio.
Chemical body protection
At some point in all the lithium-ion battery production processes, full-body chemical protection will be required – and Ansell currently offers four different PPE outfits in the AlphaTec® range. In addition, the BioClean™ 2000 Model 111 will soon be added to the range.
If you want to power-up the PPE for your own lithium-ion battery production line, talk to your usual ERIKS contact about Ansell solutions.
Tailored safety assessments
AnsellGUARDIAN® is a tailored service designed to help you create a safer, more productive and less injury-prone working environment.
Ansell safety experts, supported by data-driven methodology, will provide:
- A personalised risk management solution
- Business performance improvement advice
- PE dispensing best practice recommendations – for increased productivity and less waste.
To help you select the most effective chemical PPE solutions for your particular needs, AnsellGUARDIAN® Chemical provides a suite of digital tools.
For more information, contact your local ERIKS Service Centre, who will be happy to discuss your options.
#Ansell #ERIKS #LetsMakeIndustryWorkBetter #SafetyGloves #EVBattery #AnsellGuardian