In this article
Buses, Bugattis, Planes and Cranes - Measuring-Up To One Of Engineering's Biggest Challenges
The only way to understand the scale and challenges of some engineering jobs is to compare them with things we can all relate to. ERIKS’ refurbishment and remanufacturing of Unloader Number 3 at the Tata Steel Port Talbot plant was one of those jobs.
There are 3 harbour cranes on the dockside at Port Talbot, unloading cargoes of iron ore and coal. Unloader Number 3 has been operating since the 1960s, during which time it has lifted around 1.6 million tonnes a year, in 50-tonne buckets, with 20-30,000 bucket lifts every 12 months.
The crane’s four legs are mounted on a total of 10 carriages, running on railway lines along the dock. As the crane weighs around the same as two and a half Airbus A380 aeroplanes (900 tonnes), the carriage wheels need to be able to withstand up to 44 tonnes of load when storm conditions strike. That’s the same as five and a half fully-loaded double-decker buses. At the same time, the drive produces 27,500Nm of torque per carriage, which is the equivalent of 22 Bugatti Veyrons, or 72 two-litre VW Golf Mk VII TDIs.
With the crane operative high above the ground, dozens of people working beneath, and a ship in the harbour alongside, this is a piece of engineering demanding no half-measures, with no room for error. In other words: the perfect job for ERIKS.
Shock and ore
The operating environment on the dockside is tough for both men and equipment.
Iron ore and loose coal frequently fall from the crane buckets onto the train tracks, where the dust is picked up by the carriage wheels and makes its way into the mesh of the carriage’s spur gears. This can cause the crane to stall in motion, damaging not just the gears but – thanks to the shock load – other drive components such as the gearboxes, brakes and bearings.
Together with over 50 years’ wear and tear, and sea water corrosion, the result was frequent drive failures, high maintenance costs, and occasional fines for ships delayed in dock waiting to be unloaded while the crane was out of action.
Engineering an effective refurbishment solution was the challenge ERIKS faced. However this was made even more difficult by the need to remove two operational – rather than spare – drives to refurbish. Tata Steel would only allow the crane to be out of action for two weeks, and a test dismantle, re-weld and remanufacture of a single carriage proved this was an impossible timescale.
However, ERIKS believes in achieving the impossible. In this case, by offering to manufacture two new carriages from scratch, to keep the crane operational while the remaining carriages were refurbished.
Heavy lifting
Much of the project’s “heavy lifting” fell on the Swansea Electro-Mechanical Services division, and the Pensnett Product Business Units, all under the project management of Engineering Manager Mahesh Patel.
The project’s scope grew over time, until ultimately ERIKS, in conjunction with SKF and Fenner brands, was responsible for:
- A new drive, eliminating the highmaintenance open spur gears
- A Fenner P Series gearbox of greater efficiency than the worm gearbox drive previously in use
- An IP65 enclosed electromagnetic brake system to replace the calliper brake system, which was highly susceptible to contamination and corrosion
- A more cost-effective SKF spherical roller bearings to replace existing taper roller bearings
- New wheels, which are over 100kg lighter
The complete package
ERIKS’ complete design, engineering and manufacturing capabilities across a whole range of components not only made it possible to complete the task successfully. They also enabled real added value: a new, lighter wheel design, a more reliable electromechanical braking solution, and two completely new carriages to keep Tata Steel’s dockside operations up and running throughout.
The scale and complexity of this project was something few other companies could have taken on. For ERIKS, it was business as usual.
Savings on a massive scale
Before the ERIKS upgrade, maintenance and repairs to Unloader Number 3 were costing Tata Steel over £1,200 a week in labour alone.
Together with the cost of replacement outrigger bearings, labyrinths, pinion and intermediate gears, and repairs to the gearbox, gearbox coupling and motors, total maintenance costs for the unloader’s 10 drives were running at approximately £184,000 per annum.
Since the completion of the upgrade, savings of over £500,000 have been realised.
For more information on Power Transmission and to get in touch with one of our ERIKS Specialists, please contact your local ERIKS Service Centre, who will be happy to discuss your options.
#ERIKS #LetsMakeIndustryWorkBetter #Fenner #SKF #Engineering #Manufacturing #CostSavings