In this article
Optimising boiler houses: A sustainable journey for industry
Sustainability isn’t a destination—it’s a journey, and today we’re focusing on optimising the boiler house as part of that ongoing commitment. Energy efficiency is crucial for sustainability and cost reduction. Let’s explore how small changes can make a significant impact on the environment and your bottom line.
The Challenge of Sustainability
We’ve all seen the alarming headlines about climate change. We’re no stranger to these concerns, with rising pressure to reduce carbon footprints and energy consumption. Global targets, like those set by the Paris Agreement, call for limiting temperature rises to 1.5 degrees Celsius, reducing emissions annually, and supporting sustainable development worldwide.
But with such massive challenges ahead, it’s easy to feel overwhelmed. The question remains: What can your organisation do? The answer lies in small, actionable steps that lead to significant results over time.
The Six Rs of Sustainability: A Boiler House Focus
A great place to start is by revisiting the Six Rs of Sustainability. These principles are becoming increasingly well-known, particularly in education and research. They serve as a foundation for small changes that can lead to big impacts. Let’s see how each of the six Rs can be applied directly to optimising boiler houses in food production.
Firstly, it’s essential to start with the baseline – gathering granular data and load profiling is a non-negotiable first step, which can be achieved through the correct metering technology.
1. Reduce
Reducing fuel consumption is a straightforward way to cut CO2 emissions. But how can you reduce fuel without compromising production needs?
- Audit Energy Use: Monitor your current fuel consumption and identify areas where efficiency improvements can be made.
- Implement Efficient Control Systems: Automated controls can manage fuel use more precisely than manual operations, ensuring that fuel is used only when necessary.
2. Reuse
Think about reusing resources that are already in your system. For instance, flash steam generated during processes can often be recovered and used elsewhere.
- Recover and Reuse Steam: Integrating flash steam into other stages of production reduces the need to generate new steam, thus lowering fuel demands.
3. Recycle
In boiler systems, recycling is all about condensate. Reusing condensate means returning warm water to the boiler, reducing the energy needed to heat it back up.
- Recycle Condensate: Not only does this save on fuel, but it also reduces the consumption of chemicals needed to treat fresh water. The result? A win-win for both sustainability and costs.
4. Refuse
Don’t be afraid to challenge traditional practices. Refuse to accept outdated methods if better alternatives are available.
- Evaluate Current Procedures: Many boiler houses still rely on manual processes for safety checks, even if automatic systems are in place. Trusting and understanding the technology you have can save time, money, and resources.
5. Rethink
Reconsider how your boiler house operates. Has your business evolved? Are you still relying on old systems that might not align with your current efficiency goals?
- Reassess Load Demands: Regularly update your understanding of what your boiler needs to produce and when, ensuring that your operations are as efficient as possible.
- Measure Your Impact: Start tracking your energy use, emissions, and savings to identify trends and report progress.
6. Repair
Basic maintenance is often overlooked, but it’s an essential part of an optimised boiler house. Regularly check for leaks, insulation wear, and system inefficiencies.
- Regular Maintenance Checks: A small leak in a steam pipe might not seem critical, but over time it can waste thousands of pounds in fuel and chemicals. Simple repairs can lead to massive savings.
From Small Steps to Big Impacts: Why Optimisation Matters
Even modest changes can significantly lower fuel use and emissions. Consider these statistics:
- 1mm of Scale can increase fuel costs by 10%.
- 1mm of Soot can add 2.5% to your fuel bills.
- Increasing the temperature of a feed tank by 6°C through improved condensate return, reduces fresh water consumption, lowers chemical requirements and saves 1% on fuel.
- Fixing a 5mm hole in a steam line at 7 bar pressure could save £20,000 per year in wasted fuel.
By addressing these small inefficiencies, it’s possible to achieve up to 25% savings in boiler house costs. That’s a substantial reduction, both financially and environmentally.
Begin Your Journey with Optimisation
Optimising your boiler house is a critical first step towards broader sustainability goals like net zero. It’s about identifying easy wins that make a real difference. As you continue down this path, you’ll find new opportunities to innovate and refine your processes.
Optimising your boiler house isn’t just about technology; it’s about making the right decisions to benefit your business and the planet. Together, we can make a lasting impact.
Contact us to discuss your needs, arrange a consultation, or find out more about how we can support your goals.
For more information, contact your local ERIKS Service Centre, who will be happy to discuss your options.
#SpiraxSarco #ERIKS #LetsMakeIndustryWorkBetter #Sustainability #BoilerHouses #Optimisation