In this article
ERIKS Haydock - A Super Servo Service
Have you ever considered how your metal cutting machines create that precise motion for milling or bending those perfect lines in hard surfaces during metal fabrication processes? The answer, a specialised Servo Motor.
        
    Firstly, let us differentiate between a traditional AC motor and a servo motor. Unlike a traditional AC motor, which does not comprise of a particular assembly, a Servo motor is made up of a magnet rotor, stator and a feedback device used for position and control. The feedback device is set up in a precise position and when the motor is took apart and put back together the feedback device will need to be put back to exactly where it was originally taken – they are most commonly used in closed-loop systems.
Designed to rotate specific parts of a machine with accuracy and efficiency, a servo motor is controlled with an electric signal, which can be both analog or digital, to determine the specific amount of movement required. For example, think of a paint line at a car manufacturing plant, where the motor only needs to move a certain distance to cover its required course, with an encoder serving as a sensor that determines speed and position feedback.
As you can appreciate, operating with such complex machinery often comes with its own problems. So, when errors do arise, it’s good to know that companies such as ERIKS have the technical expertise to provide an impartial solution that will get your production back running to its most efficient.
 
Test, repair, overhaul – The choice is yours
At ERIKS we are committed to providing only the highest quality of repairs, whether that be traditional motors through to servo motors.
Our approach remains, and has since day one, that any repair or refurbishment request will be returned ‘as good as new’ ensuring that your production line will be as efficient as ever before.
Servo motor repair and testing is a specialist service that requires skills in electrical, mechanical, and electronic disciplines – a combination of skills difficult to source in today’s industry.
Backed by an experienced team of engineers with decades of knowledge and expertise, ERIKS offers an unrivalled servo motor repair service out of our specialist Haydock Regional Hub.
With the capabilities to offer support with spindle motors, water cooled generators, AC / DC servo motors, ERIKS repair capacity includes:
- Bespoke servo motor/repair cell
 - Complete fault assessment
 - Full overhaul and rewind capabilities
 - Motors stripped, tested, and aligned using
 - a Mitchel TI-5000
 - Encoders including SICK (SRS, SRM),
 - Heidenhain (ERN, EQN) and Tamagawa
 - Resolvers
 - Hall effect sensors
 - Tachometers
 
    
    
    
Unsure of specification?
With a small yet dedicated team of three specialist servo motor engineers, our Haydock facility also has the expertise and skillset to reverse engineer components utilising data sheets that are readily available online.
This means that even if you’re unsure of the correct specification for your application, our engineers can source the blueprints you need and ensure that your servo motor matches any requested specification.
Utilising an unrivalled support network, ERIKS are proud to offer a 24/7 servo motor service, with anytime call-out option, with geographical coverage capturing the entire UK. Add that to our renowned impartiality, and whether it be a simple test, complex repair, or complete overhaul, we’ll get your production line back up and running in no time.
For more information on our expert Servo Motor capabilities or to make an enquiry, contact your local ERIKS Service Centre, who will be happy to discuss your options.
#ERIKS #LetsMakeIndustryWorkBetter #Engineering #Repair #Supply #Haydock