In this article
Breathe Easy: How smart monitoring is reinventing clean environments
If you’re protecting patients in an operating theatre, preventing contamination in pharmaceutical labs, or ensuring flawless finishes on automotive paint lines, ‘clean enough’ just isn’t good enough.
Clean, controlled environments rely on consistent airflow, sealed integrity, and critical assets running at full efficiency. But wear, misalignment, and unnoticed faults can quietly compromise all of that – unless you’re watching closely.
These days, more organisations are moving beyond scheduled maintenance and adopting continuous monitoring to track system health in real time. With the right data, teams can respond faster, reduce energy waste, and extend the lifespan of vital assets.
Understanding the pressure
Maintaining airflow is a constant balancing act. In clean environments, systems are often pressurised to control air movement – either forcing contaminants out or ensuring they don’t escape. This pressure relies on fans and AHUs running consistently, even under heavy demand.
But small changes – like a worn pulley, a slipping belt, or a failed door seal – can have a ripple effect. A fan might draw more power to maintain pressure, or airflow may drop below compliant levels. These issues aren’t always visible during routine checks. That’s why tracking system behaviour, especially motor input and performance data, is proving essential.
Case study: NHS airflow under pressure
One busy NHS hospital saw airflow in its operating theatres begin to fall short of HTM 03-01 standards. Despite ongoing maintenance, its air handling units were struggling to keep up with demand. ERIKS carried out a full on-site investigation, combining mechanical inspection with system-level monitoring.
The assessment uncovered more than just worn belts. Pulley damage, misalignment, and an ageing motor were all affecting performance. As the motor struggled to keep pressure stable, energy usage spiked and airflow dipped – risking compliance and patient safety.
ERIKS replaced the drive system with a high-efficiency Fenner® belt and pulleys, added a new IE4-rated motor, and rebalanced the fan. Crucially, sensors were installed to track performance data going forward.
All of it was integrated into ERIKS’ digital monitoring system, providing the hospital’s estates team with a live picture of airflow performance and asset health. The improvement was immediate – and measurable.
One system, multiple sectors
Clean air monitoring isn’t limited to hospitals. ERIKS supports sectors from pharmaceuticals to food processing, helping businesses detect early signs of failure in critical environments. For example, in automotive paint lines, even minor air contamination can ruin product quality. Monitoring air handling units and fan behaviour helps teams act quickly, reducing downtime and waste.
In these settings, sensors can often be installed without disrupting production. Fan motors, vibration data, and thermal imaging are all used to give a clear picture of system behaviour. And where ATEX or hygiene standards apply, ERIKS supplies sealed, cleanable, and wire-free sensor options that meet strict compliance.
The impact? Fewer breakdowns, more informed maintenance planning, and confidence that environments are running as intended.
Prevention is better than cure
In maintenance, just as in medicine, early intervention saves time, money – and in some cases, lives. That’s why more organisations are moving beyond traditional break-fix approaches and scheduled servicing, embracing a data-driven strategy built around prevention.
With real-time insights at their fingertips, engineering teams can detect subtle signs of wear, misalignment, or system stress long before they lead to costly downtime or compliance breaches. No more waiting for a vibration threshold to be crossed or airflow to dip below safe levels.
Now, decisions are guided by live system behaviour and trend data – not guesswork or fixed intervals.
So when a fan motor begins drawing slightly more power than usual, or when vibration patterns change over time, condition monitoring tools like ERIKS’ Smart Asset Management (SAM) platform can flag it – long before the problem becomes visible, audible, or urgent.
In clean environments, where uptime is critical and compliance non-negotiable, prevention isn’t just better than cure – it’s essential.
What is the SAM Platform?
Smart Asset Management (SAM) is ERIKS’ digital monitoring platform, built to bring all condition data into one place. Originally developed to streamline complex survey reporting, it’s now used across sectors to monitor the health of thousands of assets.
- Live performance data – vibration, motor power, temperature, and more
- Health scoring – intuitive 1–10 scores with visual colour codes
- Condition insights – see trends, not just alarms
- Asset hierarchy – mirrors your plant layout and CMMS structure
- Export-ready – data for reporting, planning or integration
From single assets to enterprise-wide views, SAM helps engineering teams spot issues early, plan smarter maintenance, and reduce unplanned downtime.
For more information on Smart Asset Management, contact your local ERIKS Service Centre, who will be happy to discuss your options.
#ERIKS #LetsMakeIndustryWorkBetter #ConditionMonitoring #Reliability #SmartAssetManagement #AirHandlingUnits