In this article
Harnessing Condition Monitoring: How ERIKS and SKF Are Working Smarter Together
Condition monitoring is no longer just a bolt-on to maintenance. It is a cornerstone of operational reliability. But with so many tools, platforms and data sources to choose from, knowing where to start or how to scale can be a challenge.
That is where ERIKS and SKF come in. As SKF’s first authorised Maintenance Partner in the UK and Ireland, ERIKS is uniquely positioned to combine global best practice with local knowledge, helping customers navigate the complexity of condition monitoring and use it to make smarter, faster decisions.
From hardware to insight
Condition monitoring encompasses a wide range of technologies, including vibration analysis, thermal imaging, acoustic analysis and electrical discharge detection. SKF provides the foundational tools, such as IMx-1, Microlog and QuickCollect, that monitor asset condition, detect anomalies and generate detailed diagnostic data. These systems are designed for rotating equipment, with advanced sensors and analytics that allow manufacturers to track performance continuously and respond proactively.
ERIKS brings additional value by combining data gathered using SKF technology with operational signals such as pressure, flow, temperature, valve position and asset status. Through ERIKS’ Smart Asset Management (SAM) platform, customers can view real-time dashboards, receive tailored alerts and access trend analysis relevant to their specific needs.
This turns condition monitoring from a data source into a practical tool for decision-making.
The benefit of being first
The close relationship between ERIKS and SKF means new technologies are not only available to ERIKS early but are often tested and refined in collaboration with its engineers. ERIKS provides real-world feedback to SKF, helping shape the development of future monitoring platforms.
This gives ERIKS customers earlier access to new capabilities and ensures the solutions recommended reflect both the latest technologies and the specific challenges faced by UK and Irish manufacturers.
Whether it is a small-scale sensor rollout or a fully integrated monitoring programme, ERIKS and SKF provide support that grows with the customer.
A broader capability
SKF’s expertise focuses on rotating equipment, but ERIKS extends the reach of condition monitoring into other metrics required to understand pumps, valves, fans, motors and control systems. This broader application is essential in complex industrial environments, where downtime often involves interconnected systems.
ERIKS engineers use a blend of remote sensors, visual inspections, manual walkarounds and data analysis to provide a full picture of asset health. This helps identify early warning signs, manage risk and prevent disruption to operations.
The emphasis is on turning data into action. ERIKS works closely with each customer to interpret the information, highlight priorities and guide effective responses.
Scalable support at every stage
Not every business needs the same level of monitoring. That is why ERIKS offers a flexible approach, with three levels of condition monitoring support to suit different goals and resources.
The Standard level offers access to entry-level sensors and mobile notifications. The Advanced level integrates data into the SAM platform for more detailed diagnostics and forecasting. The Professional level provides a fully managed reliability service, combining condition monitoring output with ERIKS experts' ability to deliver regular analysis, reporting and on-site support.
This approach allows manufacturers to begin at a level that suits them and scale up over time. Throughout, they are supported by ERIKS' engineers and SKF’s proven technologies.
People and practice behind the platform
Technology alone is not enough. ERIKS’ services are delivered by ISO 18436-accredited practitioners who combine product knowledge with practical insight. These teams receive regular training from SKF and feedback that helps improve SKF’s tools and services.
This partnership model ensures that the condition monitoring service is constantly evolving and grounded in day-to-day operational experience.
Turning insight into control
Effective condition monitoring gives operations teams more than data. It gives them visibility, confidence and control. With the right support, customers can improve maintenance planning, reduce emergency interventions and extend equipment life.
Working with ERIKS as an SKF Maintenance Partner gives manufacturers access to a powerful combination of high-quality hardware, reliable data and expert interpretation.
Whether supporting a single line or an entire site, ERIKS and SKF help turn condition monitoring into a strategic asset: one that supports smarter maintenance and more reliable production.
For more information about SKF & ERIKS Partnership, contact your local ERIKS Service Centre, who will be happy to discuss your options.
#SKF #ERIKS #LetsMakeIndustryWorkBetter #MaintenancePartner #Axios #ConditionMonitoring #SmartAssetManagement