Blue background with a housed bearing unit and two laptop screens showing drawings and a link showing it's smart and can be monitored digitally

Housed Bearings

Stocked range extension notice

Available from our extended stocks for next-day delivery, you can depend on ERIKS to bring you more products, even faster than before.

Our investment in ERIKS new fulfilment centre at Oldbury has allowed us to extend the range of housed bearing product we hold in stock and can now supply for an early delivery next day.

 

Priority Quote Request

Our preferred partnership status with the leading manufacturers also enables us to supply larger sizes direct from their stock to ensure the fasters supply for you.

We also stock a complete range of accessories from sealing arrangements to fitting tools to make sure you have a complete solution.

Timken

  • Split roller bearings to 300mm
  • SAF Pillow blocks to 90mm
  • SNT Plummer blocks to 380mm
  • Type E housed units to 125mm

SKF

  • SNL Housings to 160mm
  • Split roller bearings to 125mm
  • Split Plummer blocks to 85mm

Schaeffler

  • SNS Split Plummer blocks to 530mm
  • SES Split Plummer blocks to 160mm

NSK

  • Self-lube to 40mm
  • Silver-lube to 40mm

Knowing your Housed Bearings

SKF SNL Housing

Sizes from 30 – 160mm bore size.

SNL plummer (pillow) block housings are the most popular SKF bearing housings on the market, developed to be the first choice for design, quality and economy. Different housing variants and seal designs are available, making the use of tailored housings virtually unnecessary and enabling cost-effective bearing arrangements to be made.

Industries: Agriculture, Building Mining and Quarrying, HVAC, Food and Beverage, Material Handling, Medical and Health Care, Packaging, Print and Paper, Utilities

Timken Split Cylindrical Roller Bearings

Sizes from 45 – 300mm bore, larger sizes available on request

A split bearing can add value to your operations by significantly reducing downtime associated with moving equipment to change out a standard bearing. Easier to install, maintain and replace, split bearings can cut operational costs, free up your resources for other tasks and remove safety risk.

Industries: Building Mining and Quarrying, Chemical, HVAC, Food and Beverage, Material Handling, Medical and Health Care, Packaging, Print and Paper, Utilities, Steel, Oil and Gas, Power Generation

NSK Self-Lube®

The Self-Lube® units are a versatile range of housings and inserts - all cast iron housings are supplied with regreasing facility, capable of taking up initial misalignment during assembly. The general housing types are pillow blocks, flange units, take-up units, cartridge units and hanger units. Suitable for a wide range of industry applications.

Industries: Agriculture, Building Mining and Quarrying, HVAC, Food and Beverage, Material Handling, Medical and Health Care, Packaging, Print and Paper, Utilities

Schaeffler (FAG) SES Split Plummer Block

Schaeffler is setting a new standard with the innovative large-size bearing housing SNS.  The new housing design distributes loads more evenly in the rolling bearing: The service life of the bearing is increased by up to 50 percent. Numerous details of the new housing design make lubrication, mounting, and condition monitoring much easier.

Industries: Agriculture, Building Mining and Quarrying, HVAC, Food and Beverage, Material Handling, Medical and Health Care, Packaging, Print and Paper, Utilities

Expert knowledge in Housed Bearings? Look no further...

Explore our solutions with SKF, TIMKEN and NSK:

Man holding hand to mouth sharing a secret

Want to hear a secret? Extended Sealed bearings lifecycles

Aggressive industries such as quarrying and mining are highly demanding. The rigorous nature of the processes. The ever-changing environment. The unpredictability. The combination of these factors makes achieving efficiency difficult, particularly when you take into consideration elements such as contamination which is unavoidable.

Yellow and silver Industrial machinery showing to conveyor lines on decorative bricks

Timken offer a time-saving new angle on roller bearings

Baking is essential for bricks – to make them solid, strong and hard-wearing. For bearings, it’s not so desirable. 

Coal Mine Excavator with claw machine scrapping coal

When the going gets tough...

Bearings keep machines and equipment moving. But what happens when everything else is doing its best to stop them?

Downloads

The NEW Know+How Hub

The new home for ERIKS News, Blogs and Case Studies - keep up to date with all the latest news and updates in one place

The latest:

There are savings in the air...

There’s a saying that what you don’t know doesn’t hurt you. But it definitely doesn’t apply to air l...

Improving electrical safety - and maintenance in seconds

Electrical safety isn’t a place to cut corners. There are strict procedures to follow to ensure the ...

Contact

Get in Touch

For all general enquiries use the Enquire Online form - we'll connect you with the best member of our team for your query.  Alternatively, look up your local service centre...

Got a Technical Question?

We are proud to boast a strong team of technical specialists in each of our product and service areas. If you have a technical question a member of our team would be happy to help. 

Share Your Thoughts

At ERIKS we strive to deliver the best quality service and products. As part of this goal we encourage customers to submit feedback on their experiences so we can resolve any issues and concerns.

ERIKS Employee