Taking a step in the right direction with Schaeffler
We are all becoming more aware of the need to protect the world from catastrophic climate change. Th...
Sometimes it’s easy to miss the big picture because you’re focussing on the small details. That’s why a failing mill classifier – essentially a “rock sorter” – caused so many problems for a plaster and plasterboard manufacturer at their site in Nottinghamshire. At least it did until ERIKS know-how sorted the problem.
ERIKS’ bearings and belts experts were called to the site when the mill classifier failed for the second time due to a collapsed bearing. Close inspection revealed that the bearing problems were only symptoms of larger issues. In fact the machine, only commissioned around 6 months earlier – had never been able to run at full output.
This second bearing failure also only just stopped short of a health and safety disaster.
The 45kW motor – weighing over 300kg – was ripped off its mountings, but fortunately hung on by a thread instead of dropping 20 feet to the ground, where a large hole would have been the least of the outcomes.
In discussions with the German OEM, it came to light that the asset was a larger version of an otherwise identical machine already in use elsewhere. However, the specification had simply been upscaled, without considering resulting increases in forces and stresses on individual components.
Compounding the problem were a number of installation errors spotted by the ERIKS engineers.
Firstly, the spherical roller bearing at the lower end of the shaft, and the spherical roller thrust bearing at the upper end, were fitted at the opposite ends to where they should have been. Severe radial load on the spherical roller thrust bearing was causing its inner ring to “climb” up the outer ring, placing extreme edge loading on the outer ring and cup. At the same time, the spherical roller bearing at the opposite end was experiencing severe axial load to the top set of rollers, which was causing spalling and – ultimately – bearing failure.
Meanwhile, because the bearings were not sitting properly in their seats, they had been over-greased: treating the symptoms rather than the cause. Flooding in grease resulted in an increased running temperature, made worse still by the incorrect positioning of the grease escape holes at the top of the bearing arrangement.
The last weak link in the chain was the power arrangement. Although the drive was only rated for 30kW, it was being driven by a 45kW motor, controlled by an inverter to run at half speed. The drive was also operating 8 budget belts which were under-rated for the power, though the OEM’s engineer was proposing to reduce these to 5.
With the current set-up of the asset, this would only have lead to more problems and an even greater risk of failures.
After their inspection, and after running the specification through the Fenner® Drive Designer, ERIKS’ engineers came up with the following recommendations:
Finally, when a fault developed on a Saturday due to a warped nut, an ERIKS engineer attended immediately and set up sensors to determine if vibration had caused the nut to loosen. When the monitoring proved this was the case, affected nuts were swapped for replacements which actually tighten through vibration.
That the customer is now getting full production from their asset with no drive issues is one testimonial to ERIKS know-how. The other is the fact that the OEM has changed the design of the machine, based on ERIKS’ recommendations.
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
We are all becoming more aware of the need to protect the world from catastrophic climate change. Th...
For all general enquiries use the Enquire Online form - we'll connect you with the best member of our team for your query. Alternatively, look up your local service centre...
We are proud to boast a strong team of technical specialists in each of our product and service areas. If you have a technical question a member of our team would be happy to help.
At ERIKS we strive to deliver the best quality service and products. As part of this goal we encourage customers to submit feedback on their experiences so we can resolve any issues and concerns.