Cost of Living Crisis? Nuclear Fuel Investment vs. Wind Power
In April, the UK Government published its long-awaited Energy Security Strategy. It was launched wit...
What sticks to a conveyor belt even more persistently than Paul Hollywood sticks to the Great British Bake Off? Bread dough. At least that’s what one industrial baker found. But fortunately ERIKS found a non-stick solution.
The two side-by-side conveyor belts causing the sticky issue are used to convey bread dough up a 60° incline, at the same time as the dough is compressed and spread out across them. At the top of the slope, a horizontal length of belting then conveys the dough to another horizontal conveyor that drops the dough into a hopper.
Instead, the dough often sticks to the PVC belting and even tries to wrap around it. The belts also tend to mistrack, meaning they last only 3-4 months each before needing replacement – which means extensive downtime. And the slippage and pulsation of the PVC belts also stretches and compresses the dough, making it uneven.
All in all, a tricky, sticky problem.
ERIKS engineers applied their know-how to find a replacement belt which would solve all the customer’s problems at once. Their answer was the Ammeraal Beltech uni M-QNB NS (Non-Stick) Modular Belt.
With a non-stick surface and reduced contact area, the belt is less easy for the dough to cling to in the first place. But it also incorporates pivoting belt hinges and a 0.5” pitch. This means the belt curves easily around the small idler rollers on the centre-driven conveyor, and is a perfect fit with the tight turns and with the scraper on the bottom of the centre-driven conveyor.
In fact, the pivoting belt hinges actually help to force the dough off the belt surface.
But while the dough slips off easily, the belts slips less.
A thicker tooth profile and deeper pockets underneath than competitive PVC belts help create better sprocket engagement and a positive sprocket drive. This reduces belt slippage, which creates a steady and consistent drive. And this in turn means there’s less stretching and compressing of the dough, for more consistent product quality.
The precise and positive sprocket engagement, combined with effective tracking, also helps to prolong the life of the Ammeraal Belt. Compared with a PVC belt, it lasts 4-6 times longer.
And then, when it eventually does need maintenance or replacement, the locking pin on the belt makes it quick and easy – unlike the extensive downtime required to replace a one-piece PVC belt.
With easier product release from the non-stick surface, and a longer service life, the Ammeraal Beltech uni M-QNB NS Modular Belt has increased production line uptime and saved the customer’s dough, in more ways than one.
Get the latest updates from ERIKS including:
Choose any or all of these via the ERIKS Subscription Centre!
Our Know+How brings together the best of the latest Know+How Hub articles in one easy to digest magazine, covering the following topics:
That's why its the leading magazine for maintenance engineers from ERIKS.
Want Know+How Magazine delivered direct to your door? Visit the ERIKS Subscription Centre to opt-in!
Take a look at our latest updates...
In April, the UK Government published its long-awaited Energy Security Strategy. It was launched wit...
For all general enquiries use the Enquire Online form - we'll connect you with the best member of our team for your query. Alternatively, look up your local service centre...
We are proud to boast a strong team of technical specialists in each of our product and service areas. If you have a technical question a member of our team would be happy to help.
At ERIKS we strive to deliver the best quality service and products. As part of this goal we encourage customers to submit feedback on their experiences so we can resolve any issues and concerns.