Setting the standards in double-screw pump technology
- Nick LeesRethinking the technical and functional principles of this sophisticated pump technology, the Frista...
How frequently does an asset have to fail before it’s not just a nuisance, but a serious issue? For one potato processor, even motors which needed a repair every three months weren’t identified as a concern. But like potatoes, ERIKS engineers have eyes everywhere and soon spotted the problem.
During regular weekly meetings with the customer, ERIKS engineers noticed that the motors used to power knife peeler machines were repeatedly being listed for repair. Closer examination of the figures revealed that each of the 24 knife peeler motors was failing on average every three months.
Necessary repairs generally included rewinds and bearing replacements, at a cost the customer clearly considered sustainable. ERIKS’ engineers thought otherwise.
With the customer’s permission to look deeper into the issue, ERIKS’ first step was to undertake a Root Cause Analysis to identify the reason for the motors’ failure.
The motors in question play a part in one of the earliest stages of the customer’s production process: powering the knife peelers used to peel thousands of potatoes a day. They operate in arduous conditions in an environment where water is widely present at all times. Built to hygienic food standards from stainless steel, the motors are vertically positioned, with the output shaft at the top.
The failure mode was quickly identified by ERIKS as water ingress, and on-site inspection revealed several factors which were allowing this to happen.
Even at first glance, ERIKS’ engineers could see that the motor bodies were poorly assembled, with rough-and-ready seams where water could potentially find a way in. In addition, cabling and glands were a basic specification, unsuitable for the wet operating environment.
Lastly, the motors vertical installation presented a flat horizontal top surface where water could collect. With only a basic seal around the shaft drive this meant that, as the shaft turned, any water which had pooled on the top of the motor would sooner or later work its way into the motor.
With a proper understanding of the root cause of the problem, ERIKS could begin to solve it. This meant ensuring water ingress to the motor was eliminated through a number of design improvement measures.
The vertical positioning of the motor allowed gravity to play a part in enabling the water to seep in around the shaft.
Changing the orientation of the motor would have required a major redesign of the entire application, but preventing water from pooling on the top of the motor was simply a matter of making the horizontal surface sloping rather than flat. Any water which landed on the motor would now tend to flow away from the shaft and down the motor’s exterior.
Using a mechanical seal around the shaft added a second layer of defence against water ingress.
Lastly, the new motor was, of course, designed to be manufactured from stainless steel to IP66 ingress protection standards.
The customer has now installed two of the redesigned motors for a trial period, and ERIKS is confident the results will lead to further replacements, as the remaining motors inevitably fail in the coming months. Meanwhile, ERIKS has been involved in discussions with the original equipment manufacturer, to identify how the benefits of the improved motor designed for this specific case can have wider implications for other applications.
One of the main reasons the customer had never taken action over the frequently failing motors was the low cost of repairs. However ERIKS engineers’ figures showed that the cost of each new motor could be recouped by savings on just three rounds of repairs over the space of around nine months.
With a potential life expectancy of several times that, the new motors will more than pay for themselves, even before taking into account cost savings on maintenance and repeated installation after repair, compared with the previous design.
Now the value of looking deeper into asset failures has been clearly demonstrated, the customer has given the go-ahead for ERIKS’ engineers to monitor downtime in relation to asset failure. Anywhere that 70% or more downtime can be attributed to 30% of assets, ERIKS will look for the root causes, and identify cost-effective solutions.
Clearly it’s not just in the potato field where a bit of digging can yield impressive results. And even if you’re not involved with potatoes, you can rely on ERIKS’ engineers’ expertise when the chips are down.
Get the latest updates from ERIKS including:
Choose any or all of these via the ERIKS Subscription Centre!
Our Know+How brings together the best of the latest Know+How Hub articles in one easy to digest magazine, covering the following topics:
That's why its the leading magazine for maintenance engineers from ERIKS.
Want Know+How Magazine delivered direct to your door? Visit the ERIKS Subscription Centre to opt-in!
Take a look at our latest updates...
Rethinking the technical and functional principles of this sophisticated pump technology, the Frista...
For all general enquiries use the Enquire Online form - we'll connect you with the best member of our team for your query. Alternatively, look up your local service centre...
We are proud to boast a strong team of technical specialists in each of our product and service areas. If you have a technical question a member of our team would be happy to help.
At ERIKS we strive to deliver the best quality service and products. As part of this goal we encourage customers to submit feedback on their experiences so we can resolve any issues and concerns.