Cost of Living Crisis? Nuclear Fuel Investment vs. Wind Power
In April, the UK Government published its long-awaited Energy Security Strategy. It was launched wit...
Heavy duty helical, bevel, worm and planetary gearboxes are among the most common pieces of equipment used in many different industrial applications, from food and beverage, pharmaceutical and quarrying, to mining, power generation and the manufacture of metals and chemicals.
Despite their widespread use and, in many applications, their critical role in power delivery and control mechanisms, they are often overlooked; until such time, that is, when they develop a fault or fail unexpectedly. An expected failure can, at best be inconvenient, and at worst, result in considerable loss of production and unplanned costs, often running to many thousands of pounds.
Gearbox faults generally stem from factors such as incorrect lubrication, poor installation or alignment, overloading and inappropriate maintenance practices. Industrial gearboxes are often subject to high levels of shock loading, vibration and extreme environmental conditions, so harsh operating conditions will rapidly exacerbate the effects caused by imbalance or wear.
An inherent feature of power transmission components has been material degradation, which leads to failure and is often exacerbated by the local environment in which the components operate. Failure of components will lead to downtime, which can be extremely costly for many industrial processes.
Wear is not the only factor to limiting the lifetime of power transmission components. The best manufacturers will advise customers to consider all the factors involved in the mechanics of each application. It’s all too easy to specify components based on breaking load, but this does not necessarily ensure that the best solution is found in terms of total service life.
Around 50% of all gearbox faults are caused by bearing failures due to excessive axial and radial loads on, for example, output shafts; similarly, over or under lubrication of bearings, or using the wrong lubricants, can cause overheating or metal-on-metal contact within each bearing.
Gearbox seals generally fail due to high levels of contamination such as dirt and other debris that accumulate around shafts; as each shaft rotates, the dirt and grit is ground into the seal, causing it to abrade. Damage can also occur if shafts are misaligned or if the gearbox is exposed to temperatures outside its operating specification, with the risk that seals will warp.
Gears typically fail due to contaminants mixing with the gearbox lubricants. Contaminants can enter through damaged seals or be produced from within the gearbox itself, for example, from particles generated by metal-on-metal wear. In each case, particles can become trapped between gear teeth, causing heat, wear and potential failure. Problems can also arise if gears have been incorrectly assembled or installed or if they become misaligned during operation due to excessive loads on rotating shafts.
Gearboxes either fail catastrophically, causing an immediate loss of power, or gradually exhibit a decline in performance due to component wear; this typically manifests itself as vibration, leading to excessive heat and noise, which should be detectable using standard condition monitoring instruments. Ultimately, even the best-maintained gearbox will eventually reach the stage where refurbishment will be required.
Although there are many gearbox repair companies, few have the skills, knowledge or resources to analyse and understand the root causes of gearbox failures. Consequently, they will replace parts on a like-for-like basis, or fit low-cost but often sub-standard components, with the inevitable result that the customer is condemned to an endless cycle of breakdown, downtime and repair.
At ERIKS, as an SKF Certified Gearbox Rebuilder, we take a different approach. Our teams have undergone specialised training with an emphasis on root cause failure analysis, bearing installation, lubrication, sealing and condition monitoring. Our objective is simple: to prevent recurring failures and extend gearbox service life.
The repair or refurbishment process begins with a full analysis of the condition of the gearbox, including all component parts, to determine the cause of failure or unexpected wear; this is generally referred to as root cause analysis. Only after a complete check of those components that could have a negative impact on bearing and gearbox service life, do we carry out the necessary repairs to return each gearbox to optimum reliability.
Our engineering teams work to exacting standards and specifications, using only high-quality components from the original equipment manufacturer, including the most advanced SKF bearings and seals. We are also regularly audited to ensure we comply with all the latest technical and quality requirements.
Our gearbox services extend beyond repair and refurbishment. We can, for example, remove and re-install each gearbox, and can upgrade older gearboxes with the latest components and lubricants to improve capability and lifetime reliability. With each
gearbox being supplied with a detailed inspection report that acts as a benchmark for future maintenance and, if specified, condition monitoring inspections.
We’ve been repairing industrial gearboxes since 1982 and have developed an unrivalled level of experience and knowledge. We now provide nationwide coverage from our custom-built engineering facilities, working to the highest quality standards to provide a timely and cost-effective service that helps customers maximise their productivity and profitability.
We’re a fully accredited SKF gearbox repairer. We work to the highest standards, using only OEM-approved components and engineering processes. We build-in quality and reliability to every gearbox, giving you total peace of mind.
Why not put us to the test? Talk to an engineer today, hit the link https://eriks.co.uk/en/pages/skf-gearbox/ alternatively, scan the QR code (right)
Alternatively, contact your local ERIKS Service Centre, who will be happy to discuss your options.
#ERIKS #LetsMakeIndustryWorkBetter #SKF #Gearbox #Rebuilder #Approved #Certified
Get the latest updates from ERIKS including:
Choose any or all of these via the ERIKS Subscription Centre!
Our Know+How brings together the best of the latest Know+How Hub articles in one easy to digest magazine, covering the following topics:
That's why its the leading magazine for maintenance engineers from ERIKS.
Want Know+How Magazine delivered direct to your door? Visit the ERIKS Subscription Centre to opt-in!
Take a look at our latest updates...
In April, the UK Government published its long-awaited Energy Security Strategy. It was launched wit...
For all general enquiries use the Enquire Online form - we'll connect you with the best member of our team for your query. Alternatively, look up your local service centre...
We are proud to boast a strong team of technical specialists in each of our product and service areas. If you have a technical question a member of our team would be happy to help.
At ERIKS we strive to deliver the best quality service and products. As part of this goal we encourage customers to submit feedback on their experiences so we can resolve any issues and concerns.