Cost of Living Crisis? Nuclear Fuel Investment vs. Wind Power
In April, the UK Government published its long-awaited Energy Security Strategy. It was launched wit...
Extensive testing has suggested that a large amount of energy required in a pump was to overcome the resistance in the pump and used to fill dead space in the air chambers. While another major issue is pumps stalling when turned down to lower air pressures to save energy or being pumped against a closed valve.
When measuring the performance of Tapflo's new TC Series against conventional AODD pumps, up to 70% in energy savings can be achieved.
Utilising patented LEAPⓇ (Low Energy Air Pump) Technology, the minimum operating air pressure is reduced by reducing internal losses and friction found in traditional AODD pumps.
The TC Series is able to start pumping at 0.3 bar with no stalling, where others simply failed to event start.
TC Intelligent pumps can be retrofitted to any existing Tapflo AODD pump, and offer an improved lifespan using an air valve over rubber seal technology, while maintenance times are also improved as the main air valve can be changed in under two minutes without the removal of the pump from the process line.
Other features and benefits include:
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
In April, the UK Government published its long-awaited Energy Security Strategy. It was launched wit...
For all general enquiries use the Enquire Online form - we'll connect you with the best member of our team for your query. Alternatively, look up your local service centre...
We are proud to boast a strong team of technical specialists in each of our product and service areas. If you have a technical question a member of our team would be happy to help.
At ERIKS we strive to deliver the best quality service and products. As part of this goal we encourage customers to submit feedback on their experiences so we can resolve any issues and concerns.