Posted at Tuesday, 07 January, 2020

Understanding Zinc and Zinc-Like Coatings with Ambersil

Paul Skade
By James Goodgame
Lubrication Product Manager, ERIKS UK & Ireland

I came to ERIKS UK towards the end of 2014 following a few years working in the business media and advertising industry. I started in the branch support team, lea...

Read full bio

Corrosion is an ever-present problem for all ferrous metals, there are many methods to guard against it. ERIKS and Ambersil aim to demystify zinc and zinc-like coatings.

 

Different anti-corrosion coatings are selected to fulfill application-specific criteria, but all can be braodly categorised as either

  • A barrier coating that isolates the steel substrate from both moisture and oxygen, or
  • A cathodic coating that corrodes in preference to steel

 

Within these two categories, there are many products - manily in the barrier type - and all can be categorised as either "short term temporary" or "long-term permanent".

Why zinc?

At the top end of the protection spectrum, molten zinc is used in the hot-dip galvanising process that physically bonds zinc to a steel substrate.

The process provides exceptional protection to the steel not only because the steel is entirely covered by a barrier of zinc - isolating it from rain, salts and corrosive elements - but also, because zinc corrodes in preference to the steel, providing either cathodic protection.

The 'cathodic protection' that the zinc provides is a weak electromechanical current to the steel, restricting the ionic exchange in the corrosion process.

As the zinc corrodes - in preference to the steel - it forms zinc oxide then (In the presence of moisture - a zinc hydroxide patina which further protects the steel. This sacrificial process continues until the pure zinc has reacted, at which point the steel begins to corrode.

Types of zinc

When taling about zinc and zinc content, it is important to understand the different types of zinc and the performance characteristics of each:

  • Zinc Powder - pure zinc used for cathodic protection in coatings and paints. Corrodes in preference to the steel substrate, providing a acrificial protective coating.
  • Zinc Oxide - combines good adhesion with excellent opacity and a smooth surfae for over-coating with a paint topcoat. Also demonstrates good anti-corrosion performance.
  • Zinc Phosphate - Excellent adhesion improver for difficult surfaces, frequently found in 2-in-1 paints as a primer component.

 

Testing for corrosion performance

All coatings can be tested to standardised methods detailed in ISO 9227 & ASTM B117 (salt and spray test). The results of these tests indicate the performance of a coating under laboratory conditions, in an aggressive/accelerated process. In order to bridge the gap between laboratory conditions and real world performance, ISO 12944-2 categorises product based on sustainability for specific environmental conditions: from C1 to C5 (marine). Many aerosol pack coatongs fit into category C3.

 

Formulating the right product for right-first-time results

Occasionally Ambersil are asked for a 99.9% zinc spray, or if ther zinc sprays contain 99.9% zinc. The question stems from the claim many zinc sprays make, that zinc in their products is 99.9% pure, rather than the actual content itself. The International Standard fro purity is ISO 3549, and it specifies that the minimum purity level of the zinc poweder to provide effective cathodic protection should be >98%.

 

For an effective anti-corrosion product to function as required, a compromise must be made between the various components of the formulation to ensure that specific application criteria are met. For cathodic protection products, ISO 1461 specifies a minimum zinc content in the cured film. However, there must also be adequate resin binder to ensure that the vital zinc powder adheres strongly to the surface, with good flexibility, and resistence to cracking.

Selecting the right product

Each product in the Ambersil anti-corrosion range - including 2-in-1 paints, and acrylic topcoats - has been formulated to meet a apecific application, from full actodic protection, rapid drying, to aesthetic matching.

Each  product offers different performance characteristics, and so it is important for engineers and specifiers to select the right products - or combination of products - for the best results.

 

Related Articles

Join the Conversation

Subscribe to our News, Products & Services

Latest Articles

Take a look at our latest updates...

ERIKS and Henkel make a firm bond

Jon Whitehouse

Corrosion, erosion, cavitation and mechanical damage all cause wear to pump castings, impellers and ...

Full steam ahead - Scottish distillery with Grundfos

Nick Lees

There’s steam and there’s high-quality steam. There are pump solutions and intelligent pump solution...

How to Contact ERIKS

Get in Touch

For all general enquiries use the Enquire Online form - we'll connect you with the best member of our team for your query.  Alternatively, look up your local service centre...

Got a Technical Question?

We are proud to boast a strong team of technical specialists in each of our product and service areas. If you have a technical question a member of our team would be happy to help. 

Share Your Thoughts

At ERIKS we strive to deliver the best quality service and products. As part of this goal we encourage customers to submit feedback on their experiences so we can resolve any issues and concerns.

Chat
Chat