In this article

Serving up the recipe for efficient bearings

There's no taste quite like that of a freshly baked batch of crumpets - crispy on the outside, soft and fluffy at the centre. But bearings don't feel the same about the glorious gooey consistency of batter mix as we do. And one well-known bakery found this out the hard, and costly way.

crumpets-and-melted-butter

 

Alarmingly, and inconveniently, the customer was experiencing failures every 4-6 weeks, costing in excess of £2,000 each time. But just one phone call to ERIKS' bearing specialists, and it was only a matter of time before the recipe for efficiency was served up.

Current sealing solution take a battering

The initial inspection quickly revealed that the problem stemmed from seals not performing their duties correctly, allowing the ingress of batter mix into the bearing assembly.

Normally, when leaving the mixing bowl, the batter's next destination would be a baking tray then into a hot oven, but these batches had completely different ideas.

Entering the assembly through the drive's front cover, the residue continued to build up in the unit. Passing through the outer cover seal, a mechanical seal and two inner PTFE rotary shaft seals, the bearings were inundated with gunky batter.

It had travelled all the way through the bearing assembly right to the back cover, and its abrasive consistency resulted in the rotary shaft seals being extremely worn. Even with four layers of sealing technology, the pressure exerted by the batter mix was too overwhelming for the various seals types.

Investigations began

ERIKS' bearing division got to work, and the first port of call was to re-design the seal arrangement, including upgraded bearings, a complex labyrinth seal arrangement replacing the mechanical seals, and new PTFE seals, the latter being a request of the customer.

 Unfortunately, this wasn't the answer. Three months later, failure struck again. The Beta drive was re-inspected, and just like previously, the seals had once again failed.

Redesigning the sealing arrangement 2.0

Standard nitrile rubber rotary shaft seals were then installed, with a Gamma seal over the top of the assembly. As it was mounted to the shaft, and seated flat to the top cover, it would rotate simultaneously, acting as a flinger and forcing the batter away from its previous point of ingress.

As it runs flat on the top cover face, the more pressure exerted from the batter, the better it would seal, adding that extra layer of protection.

Simalube-automatic-lubricator-bearing
eriks-bearing-rotary-shaft-gamma-seal-cad-drawing

Simalube Simgle Point Lubricators were also installed, with OKS 404 high-temperature and high-performance grease lubricating the bearings.

Along with ROCOL Food Grade semi-fluid grease keeping the labyrinth clear by maintaining it under positive pressure, to combat the pressure being exerted by the batter.

The introduction of the single point lubrication systems was a smart one, delivering multiple benefits to the customer. The ingenious design provides precisely calculated automated lubrication, continuously, from one month to a full year, ensuring that grease is served consistently at the right levels and to those hard-to-reach points.

This, in-turn, would extend the lifecycle of the bearings, increase profitability through reduced downtime, and minimise the requirement for maintenance sources with its fully-automated design.

Oh, and it's environmentally-friendly and 100% recyclable. So, not only did it save the customer time and money, in the long run, it protects the planet.

Risen to the challenge

Reporting back 18 months on, the customer confirmed that the unit has been in full production without any issues. A far cry from the previous 6-week stoppages.

Since completion, two additional Beta Drive versions have been re-designed, and two further are in the process, although they slightly differ in design.

It's been an on-going issue suffered by many bakeries across the country, with ERIKS bearings specialists facing four different designs in recent times. But while it was not a simple fix, they have redesigned the sealing and bearing arrangements for all of them.

Once again, ERIKS' know-how and expertise 'battering' a problem with a well-conceived bespoke solution.

 

For more information on our Bearings and Lubrication solutions and our Sealing capabilitiy and to get in touch with one of our ERIKS Bearing & Lubrication Specialists or Sealing Application Engineers, please contact your local ERIKS Service Centre, who will be happy to discuss your options.

#Simatec #Rocol #OKS #Bakery #FoodandBeverage #Bearings #Lubrication #Redesign #ERIKS #ERIKSUK #LetsMakeIndustryWorkBetter